Open topic with navigation
Project Structure Guidelines
Introduction
By implementing a predefined structure for new projects, KAS tries to achieve the following goals:
- Efficiency in developing new applications
- High flexibility to keep only functionalities that are needed and to create the new ones that are required
- Safe applications due to an already tested and approved structure that optimize the resources usage (memory and processor load)
- Reliable framework that supports error, state, data and communication management
- Easier to exchange applications
- Less time needed to understand, maintain and teach an application (from a troubleshooting and support standpoint)
- Less documentation work is required since the main behavior of the Application is already documented (only the specific functionalities need some additional work)
|
|
Copyright © 2015 Kollmorgen™
|
|
|
Open topic with navigation